Configure GPIO using Full chip simulation for MC9S12XEP100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure GPIO using Full chip simulation for MC9S12XEP100

ソリューションへジャンプ
3,518件の閲覧回数
ughadge
Contributor II

Hi , I am new to codewarrior tool 

I want to test my GPIO code using Full chip simulation for MC9S12XEP100.

How to do so ?

0 件の賞賛
返信
1 解決策
3,452件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

to simulate gpio in full chip simulation mode, you need use CW5.x to debug code  and set connection as full chip simulation mode 

pastedImage_1.png

you can check GPIO register location in debugger memory window.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,453件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

to simulate gpio in full chip simulation mode, you need use CW5.x to debug code  and set connection as full chip simulation mode 

pastedImage_1.png

you can check GPIO register location in debugger memory window.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,452件の閲覧回数
ughadge
Contributor II

Thank you 

0 件の賞賛
返信
3,452件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信