Config PTIL_PTIL1 as input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Config PTIL_PTIL1 as input

1,855 次查看
nxp14
Contributor I

I need help with the config of PortL by the 12ZVCA192 with 48 Pins

I will use the PTIL_PTIL1 as normal digital input. but it dosent work. i have always a low on this pin.

This input detec a resistor. it is set, the pins is on low. with out it shuod detec a high over intern pullup

but nothing chance when i switch the Polaity select from Pulldown to pullup in CodeWarrior Hardware selektion

i set it to digital Input

what can i do ?

0 项奖励
回复
1 回复

1,811 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I would like to recommend to look at the section "2.5.5 Open Input Detection on PL[1:0] (HVI)" and "Figure 2-36. Digital Input Read with Pullup Enabled" in RM rev 12.1. Also, please, check if registers are correctly set.

I hope it helps.

Best regards,

Diana

0 项奖励
回复