Command converter configuration.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Command converter configuration.

2,423 次查看
fredriklund
Contributor I

Hi,

I'm trying to use a codewarrior USB utap on windows 10.

When I open the CCS.exe and type "show cc" I get the message:

"There are no command converters configured".

I type "config cc utap" and now when I try "show cc" I get:

"0: USB TAP (JTAG) (utap) CC software ver. {1.3}"

as expected, and everything is working as it should.

However, if the computer is restarted, sleeps or CCS.exe is run again, I'm back to square one.

 

Is there a way I can make sure it retains its configuration?

Appreciate any help or suggestions.

标签 (1)
1 回复

2,092 次查看
fredriklund
Contributor I

About 5 minutes after posting I found the answer.

After getting the right configuration I typed "config save".

Now it works even after a restart.