Coldfire V1 MAC simulation in Code Warrior v5.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire V1 MAC simulation in Code Warrior v5.9

ソリューションへジャンプ
2,779件の閲覧回数
davecurtis
Contributor I

Code Warrior (v5.9.0) seems to be able to assemble MAC instructions if you select a Coldfire processor that supports MAC, but the simulator crashes if you attempt to execute them.  The simulator 'set derivative' menu does not seem to include any instances of processors that support MAC.  Is this a limitation of the simulator, or is there some setting I am missing?  If it does not support MAC, is there some later version or upgrade that does?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,607件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

I have been informed me that the Simulator does not support the MAC unit and that there are no later versions that support this. I would recommend that you try using actual hardware for testing MAC instructions.

I apologize for the inconvenience.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,607件の閲覧回数
davecurtis
Contributor I

OK, maybe 'crash' is not the right word.  It jumps to startup code, probably indicating an illegal instruction trap.

0 件の賞賛
返信
2,607件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

Have you tried testing if you are able to execute the MAC instructions without using the simulator?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信
2,607件の閲覧回数
davecurtis
Contributor I

Yes it seems to work in hardware (via BDM).  Just not the software simulator.

0 件の賞賛
返信
2,608件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

I have been informed me that the Simulator does not support the MAC unit and that there are no later versions that support this. I would recommend that you try using actual hardware for testing MAC instructions.

I apologize for the inconvenience.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信