Coldfire V1 MAC simulation in Code Warrior v5.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Coldfire V1 MAC simulation in Code Warrior v5.9

跳至解决方案
2,786 次查看
davecurtis
Contributor I

Code Warrior (v5.9.0) seems to be able to assemble MAC instructions if you select a Coldfire processor that supports MAC, but the simulator crashes if you attempt to execute them.  The simulator 'set derivative' menu does not seem to include any instances of processors that support MAC.  Is this a limitation of the simulator, or is there some setting I am missing?  If it does not support MAC, is there some later version or upgrade that does?

标签 (1)
0 项奖励
回复
1 解答
2,614 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

I have been informed me that the Simulator does not support the MAC unit and that there are no later versions that support this. I would recommend that you try using actual hardware for testing MAC instructions.

I apologize for the inconvenience.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,614 次查看
davecurtis
Contributor I

OK, maybe 'crash' is not the right word.  It jumps to startup code, probably indicating an illegal instruction trap.

0 项奖励
回复
2,614 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

Have you tried testing if you are able to execute the MAC instructions without using the simulator?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复
2,614 次查看
davecurtis
Contributor I

Yes it seems to work in hardware (via BDM).  Just not the software simulator.

0 项奖励
回复
2,615 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dave,

I have been informed me that the Simulator does not support the MAC unit and that there are no later versions that support this. I would recommend that you try using actual hardware for testing MAC instructions.

I apologize for the inconvenience.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复