Codewarrior for MC68HC908GZ8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior for MC68HC908GZ8

3,335 Views
gilmar
Contributor I

Hi,

I use the Codewarrior for MC68HC908gz8 and I installed the codewarrior V11.0 and It doen't have the MC68HC908gz8. How I use MC68HC908gz8 with codewarrior ?

I have the licence for codewarrior V6.3 but doen't work with windows 10.

Best regards.

Gilmar

0 Kudos
Reply
3 Replies

3,105 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

MC68HC908gz8 is HC08 device which is only supported by CW6.3.

CW6.3 doesn't support 64bit win7/10 platform.

the officially recommendation is using CW6.2 on 32bit windows xp.

We have user provide unofficial method of install CW6.3 on win10 64bit.

How-to Directly Install CodeWarrior 6.3 Classic in Windows 7 and 10 x64 (Unofficial Method) 

You can refer it but NXP doesn't provide technical support of it. Thanks for your understanding.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,097 Views
gilmar
Contributor I

Hi,

Thank you.

I installed and is work well.

Best regards.

*Gilmar Ribeiro de Oliveira *

Supervisor de Engenharia de Pesquisa e Desenvolvimento - P&D

Tel: 55 35 3471.2555 Ramal: 0218

[email protected]   www.sense.com.br

Av. Joaquim Moreira Carneiro, 600 - Santana

CEP: 37540-000 - Santa Rita do Sapucaí/MG Brasil

Em 22/11/2018 01:59, ZhangJennie escreveu:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Codewarrior for MC68HC908GZ8

reply from ZhangJennie

<https://community.nxp.com/people/ZhangJennie?et=watches.email.thread>

in /CodeWarrior Development Tools/ - View the full discussion

<https://community.nxp.com/message/1083038?commentID=1083038&et=watches.email.thread#comment-1083038>

>

0 Kudos
Reply

3,097 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

0 Kudos
Reply