Codewarrior V4.7 can no longer load cpu beans

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior V4.7 can no longer load cpu beans

2,205 次查看
AndersJ
Contributor IV

Suddenly after a long period of perfect operation

Codewarrior fails to read the cpu bean from the project file(s).

This happened today, the first day after the holidays.

I get the same problem on ”other” computers as well.

I have tried various older generations taken from backups.

Therefore I do not believe I have corrupted files.


Could there be a date related issue with licensing, CW, Windows or something else?

What may cause this error message:

”Error during loading beans ”bean-name” from project file.

Attempting to open the non initialized bean, I get:

”Internal error: CPU database initialization failed (previous initilization attempt failed)”

What may trigger these error messages?

0 项奖励
回复
1 回复

2,131 次查看
AndersJ
Contributor IV

It seems to happen when Windows updates itself.

After uninstall of the the most recent updates, all works again, until the next update.

Has anyone seen this, or have an explanation?

0 项奖励
回复