Codewarrior V10.6 evaluation version usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior V10.6 evaluation version usage

2,037件の閲覧回数
bhuvaneshwaran
Contributor I

My Name is Bhuvaneshwaran working for Rane Madras Limited, Chennai (TN) India. We are planning to use Code warrior version 10.6 evaluation version for our project. for using S9KEAZ128AMLH controller I think we can use it for the period of 30 days. Please let me know whether we can use it for more than 30 days. Also let me know the limitation of usage of CW in the evaluation version.

ラベル(1)
0 件の賞賛
返信
1 返信

1,701件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Bhuvaneshwaran,

CodeWarrior for MCU V10.6 is the last version.

It integrates the development tools for the :

                ColdFire®, ColdFire+, DSC, Kinetis, Qorivva, RS08, S08 and S12Z architectures

into a single product based on the Eclipse open development platform.

The evaluation version include a 30 days professional license file.

We can extend the evaluation 1 time.

For details please have a look to:

     How to extend my evaluation license file for CodeWarrior

You can download the evaluation from our web site:

    Evaluation Software|NXP

By default the MCU v10.6 is running at Special Edition which is free of charge.

When the evaluation time expires the tool continue to work at Special edition.

What are the restriction ?

Please have a look to

    CodeWarrior Suites (Bas, Stand, Pro)|NXP

You will see the differences between Special edition, Basic, Standard and Professional Suite.

There is a mistake in this dialog. The first column is Special Edition and not Evaluation.

The Evaluation license file is a Professional license limited to 30 days.

Hope this will help.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信