Codewarrior + MC9S12XEP100 + External Bus Interface (EBI)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior + MC9S12XEP100 + External Bus Interface (EBI)

2,365 次查看
leandromaia
Contributor I

I'm designing a system with these main components:

  • CodeWarrior latest version
  • MC9S12XEP100 microcontroller
  • Memory Cypress CY7C1041GN (256K x 16b)

 

I've a lot of information about hardware interface and registers but few about CodeWarrior Project settings.

A simple schematic was attached in order to illustrate what I'm trying to do.

The chosen memory can be easily controlled by uC signals but I don't know how to make my code address correctly using FAR key word.

 

Following uC datasheet, AN2708 and AN2992, I got these registers values:

 

EBICTL0 : 0x33
--------
||||||||
|||+++++- ASize: 10011 - External Address Bus Size (19 lines)
||+------ HBDE : 1 - High Data Byte Enabled
|+------- 0    : 0 - Always 0
+-------- ITHRS: 0 - Reduced Input Threshold disabled (Standard Level on all pins)

EBICTL1 : 0x00
--------
||||||||
|||||+++- EXSTR0: 000 - External Access Stretch Option 0
||||+---- 0     : 0 - Always 0
|+++----- EXSTR1: 000 - External Access Stretch Option 1
+-------- 0     : 0 - Always 0

MMCCTL0 : 0x0C
--------
||||||++- CS0 : 0x00 - Chip Select 0 Disabled
||||++--- CS1 : 0x11 - Chip Select 1 Enabled
||++----- CS2 : 0x00 - Chip Select 0 Disabled
++------- CS3 : 0x00 - Chip Select 0 Disabled

MODE : 0xA0;
--------
|||+++++- 0 : 00000 - Sempre 0
+++------ MOD[C:A] : 101 - Normal Expanded Mode

 

Suppose I have a program segment that needs to be completely fitted inside 200000h–3FFFFFh.

I know I can use absolute address and set a variable at that address.

But how can I do it automatically for variables and code?

 

Today I have a project using EBI with HCS12DP512.

In this project, I set PRM file and everything was ok because my External Memory is only 16KB.

PPage was not necessary and my code was treated like an internal firmware.

However, in this new project, I need that every single access use the correct PPage.

 

Thanks.

标签 (1)
0 项奖励
回复
1 回复

2,147 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- There is a External bus  design demo and DOC :

S12XD, S12XE - External BUS design - Addendum To AN2708 

- There is a FAR Keyword demo as Jennie support:

PPAGE Use Problem. 

Hope it helps

Alice

0 项奖励
回复