Codewarrior Development Studio for HCS12(X) V4.7 Installation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Development Studio for HCS12(X) V4.7 Installation error

1,830 Views
Friends
Contributor I

Hi. I'm going to use freescale at my company. I opened installation wizard, set Destination Folder and Setup type(Complete), and clicked install button. But no installation procedure has further been progressed.

Installation Wizard said "The wizard was interrupted before CodeWarrior Development Studio for HCS12(X) v4.7 could be completely installed. Your system has not been modified. To complete installation at another time, please run setup again"

Are there any solutions about this error???

My computer uses Window7 32bit. PLEASE HELP!

 

Thank you

SeungTaek, HONG

 

0 Kudos
Reply
1 Reply

1,824 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please refer solution in this link

https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-...

However, CW4.7 is not for win10 platform. we don't have full test on it. Our suggestion is to use CW5.x instead.

 

Best Regards

Jun Zhang

0 Kudos
Reply