Codewarrior 10.5 licensing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.5 licensing

ソリューションへジャンプ
3,265件の閲覧回数
rahul011189
Contributor I

I am using Code Warrior 10.5 for P4080DS. When I try to Run or Debug my application (via Run -> Run configurations or Run-> Debug configurations), I get a debugger licensing error.126699_126699.pngDebugger license error.png

 

I tried registering my product to generate an Appropriate license as well but the NXP website throws another error saying:

"The software licensing and registration system is currently experiencing an unexpected error. Please try again or contact technical support"

 

Please help me to fix the license issue.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,049件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Rahul,

Sorry for the delay.

I've found some problem with the web license system in case of Eval registration.

I've reported the problem and it should be solved soon.

I've generated a license for you.

Rename the attached file to license.dat.

The license file includes CW for PA V10.5 windows & linux and Additional Architect Level Features (DDR, Serdes, ...)

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,049件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Rahul,

Just checked under your account and found the CWX-ARCHT-EX_xxxxx registration.

This is an evaluation which will expire the January 30, 2016.

To generate the license file I need you Disk ID vol C:.

Please provide me the DiskID.

I will send you am email including the license files.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,049件の閲覧回数
rahul011189
Contributor I

Hi Pascal,

I am not sure what do you mean by disk ID. Are you referring to the hard disk UUID on which my Linux root is mounted?

If yes, this is what I get on my terminal:

/dev/sda1: UUID="de3229b4-7ea5-4bde-880c-c1c1d075a8c8" TYPE="ext4"

Regards,

Rahul

0 件の賞賛
返信
3,049件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Rahul,

For linux we need the Ethernet address.

Q: How can I get the Ethernet Address from a Linux PC?

  1. Launch a Terminal window
  2. Run /sbin/ifconfig eth0
  3. Copy the HWaddr string (12-digit value)


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,049件の閲覧回数
rahul011189
Contributor I

The HW addr is :

HWaddr c8:9c:dc:a2:a7:8d

Thanks,

Rahul

0 件の賞賛
返信
3,050件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Rahul,

Sorry for the delay.

I've found some problem with the web license system in case of Eval registration.

I've reported the problem and it should be solved soon.

I've generated a license for you.

Rename the attached file to license.dat.

The license file includes CW for PA V10.5 windows & linux and Additional Architect Level Features (DDR, Serdes, ...)

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,049件の閲覧回数
rahul011189
Contributor I

Hi Pascal,

The licensing issue is resolved with the file you attached in your last response.

Thank you so much for the help.

But I have into another problem regarding generation of AppTRK.elf.

I am following the steps mentioned in the following file, but I am getting some errors:

/CodeWarrior_PA_10.5.0/PA/PA_Tools/AppTRK/apptrk/INSTALL

Am I looking at the right files or do I need to generate AppTRK using bitbake?

Really appreciate your help.

Thanks,

Rahul

0 件の賞賛
返信