Codewarrior 10.4 updation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.4 updation

1,502件の閲覧回数
anand_s
Contributor III

Hi all,

       We are currently using codewarrior 10.4 , MQX 4.0.2 and K60 controller. Now we have to change K60 to K66 series, so that we have to update MQX as well as Codewarrior. my question is how to update codewarrior 10.4 licensed version to latest one which support K66 series. 

thanks,

code warrior  , #k series‌ , #mqx

0 件の賞賛
返信
1 返信

1,389件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Anand,

MQX 4.0.2 was developed to work with CW MCU v10.4 and CW MCU v10.5. It has been tested and confirmed to work with CW MCU v10.6.

To update CW10.4, you just need

- uninstall CW10.4

- reinstall new version of CW

- install MQX for the new version CW.

However K66 is not supported by MQX4.x, but MQX 5 instead. This problem is not on CW side but MQX side.

Please note: If user develops new project, we don't suggest use MQX , our recommded SW is MCUXpresso IDE + MCUXpresso SDK

Welcome | MCUXpresso SDK Builder 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信