CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior

1,920 次查看
new1979
Contributor I
  • CodeWarrior USB TAP  install  drive program  ,CodeWarrior USB TAP still red light glitter,why?
0 项奖励
回复
3 回复数

1,807 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ,

What's your chip part number?

Jennie Zhang

0 项奖励
回复

1,807 次查看
new1979
Contributor I

MC56F8345VFGE

发自我的 iPhone

在 2019年1月9日,10:11,ZhangJennie <[email protected]> 写道:

NXP Community

Re: CodeWarrior

reply from ZhangJennie in CodeWarrior Development Tools - View the full discussion

Hi ,

What's your chip part number?

Jennie Zhang

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Development Tools by email or at NXP Community

Following Re: CodeWarrior in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

>

0 项奖励
回复

1,807 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Fangfeng,

USB TAP driver is included in CodeWarrior install folder. But please note, if you use 64bit win7/win10, I suggest you use CW10.x or CW11.x for programming. Classic CodeWarrior 8.3 doesn't support 64bit win7/win10 platform.

when you connect USB TAP with PC only, TX/RX is blinking (red), this is normal.

after downloading code, you should see TX/RX blinking (yellow and green), RUN/PAUSE led is on (red)


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复