CodeWarrior v7.1 debugger variable window problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior v7.1 debugger variable window problems

1,304 Views
michaeld
Contributor II

I am having issues modifying/viewing all variables currently in scope while running the debugger.  The debugger shows 'unknown error' for certain variables that are currently in scope.

 

Example function:

uint32 GetFractionalMultiplier(uint32 data)

{

     int32 tempFraction = 0;

     uint32 fractionalMultiplier = 1;

     uint32 orderOfMagnitude = 1;

 

     tempFraction = GET_FRACTIONAL_PART(data);

     orderOfMagnitude = 1;

 

     while (0 != tempFraction)

     {

          tempFraction = (tempFraction / 10);

          orderOfMagnitude = (orderOfMagnitude * 10);

     }

 

     fractionalMultiplier = (FLOAT_MULTIPLIER / orderOfMagnitude);

 

     return fractionalMultiplier;

}

 

At all points while stepping through this function, orderOfMagnitude shows `unknown error X100428X`  where X is some strange character that I don't know how to type.  The address is also blank.

 

If I use the View -> Registers tool while stepping through the function, I can see D2 getting set to 0x0000001 just prior to the while loop, and guess that is where the processor is setting orderOfMagnitude.  To confirm this, I set D2 to 0 after the while loop and got a divide by zero exception.  But why should I have to guess which register is being used in order to modify the value?

 

Debugging an MCF52211, 16K version.

Labels (1)
0 Kudos
Reply
0 Replies