CodeWarrior for MPC5748G?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for MPC5748G?

ソリューションへジャンプ
2,177件の閲覧回数
coderunner50
Contributor II

Hello, I just purchased a Qorivva MPC5748G dev kit (MPC574XG-MB and MPC574XG-324DS) and don't have the CodeWarrior MCU 10.6 project files (header, linker, .mem, etc.) for this specific part. I also have a USB Qorivva Multilink debugger that I have used with the MPC5646B/C eval board. Are there any plans to have a CodeWarrior update or version that works with the MPC5748G? Also, besides Green Hill Software Multi are there any other development packages currently available to evaluate this part? Best Regards.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,834件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Jim,

Unfortunately the MPC57XX is not supported on MCU V10.6.

At this time there is no plan to support this family.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,835件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Jim,

Unfortunately the MPC57XX is not supported on MCU V10.6.

At this time there is no plan to support this family.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信