CodeWarrior for Linux - Component Inspector properties window is blank

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for Linux - Component Inspector properties window is blank

1,678 Views
fweller
Senior Contributor I

The component inspector properties window for DDR is blank.  This window was previously filled with register settings, and had been working properly for the past week.  Today after a few restarts of CW, the DDR properties window became blank.  I have tried rebooting a few times, also tried making a new project, also tried a different license file, nothing works.  Here is the strange thing: I am able to run DDR validation on the board, and I am able to view the configuration registers.

How do I get the DDRv component inspector properties to show the DDR settings again?

CodeWarrior Development Suite for Networked Applications.  CodeWarrior Development Studio for QorIQ LS series for ARM v8 ISA

Version: 11.5.2 Build Id: 210130

My OS is Ubuntu 20.04 LTS

Screenshot below

ComponentInspectorBlank.png

 

0 Kudos
Reply
1 Reply

1,658 Views
yipingwang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply