CodeWarrior for HCS12(X) Microcontrollers v5.2 Eval

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for HCS12(X) Microcontrollers v5.2 Eval

Jump to solution
3,272 Views
tnriley
Contributor III

I am looking for a downloadable  eval copy of CodeWarrior for HCS12(X) Microcontrollers v5.2. I have a non-networked development machine that requires installation from a DVD,etc. Please advise, Thanks, TIm

Labels (1)
0 Kudos
Reply
1 Solution
2,477 Views
tnriley
Contributor III
0 Kudos
Reply
3 Replies
2,478 Views
tnriley
Contributor III

pastedImage_1.png

0 Kudos
Reply
2,477 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

in addition, this is evaluation CWs (include CW5.2) download link:

Evaluation Software|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,477 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tim

You  can first download the installer in the PC which can connect to internet ,

then copy the installer package into U disk , then use it to install on the non-networked development machine .

Does this can help ?


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------