CodeWarrior command line interface for download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior command line interface for download

ソリューションへジャンプ
3,009件の閲覧回数
hyunuk_ha
Contributor I

Dear ZhangJennie‌, 

I succeedded compile my project using your article as attached. 

But is there any way to,

1. Automated download way( using command line interface), or

2. Download command line interface(Attached document includes compile process only)

Please help me with an urgent and important issue.

My project is PIL(Processor In the Loop) simulation based on simulink platform.

Thank you in advance.

Regards,

Hyunuk

# codewarrior‌ , commandlineinterface‌

ラベル(1)
1 解決策
2,886件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hyunuk,

Professor Erich Styger ever wrote article about CodeWarrior Flash Programming from a DOS Shell.

CodeWarrior Flash Programming from a DOS Shell | MCU on Eclipse 

Please check if this can help you.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,886件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hyunuk,

Professor Erich Styger ever wrote article about CodeWarrior Flash Programming from a DOS Shell.

CodeWarrior Flash Programming from a DOS Shell | MCU on Eclipse 

Please check if this can help you.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------