CodeWarrior USB TAP 900-75115 REV G compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior USB TAP 900-75115 REV G compatibility

1,581 Views
ainsoftinc
Contributor I

Hello,

Is the CodeWarrior USB TAP 900-75115 REV G compatible with the MPC860 chip for BDM, programming and also reading the FLASH?

Thank you.

0 Kudos
Reply
1 Reply

1,342 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Michael Michael,

Please refer to USB TAP for MPC8xx from USB TAP for PowerQUICC® I|NXP , it seems that the USB TAP which you mentioned is for e300 and e500 processor. Please refer to the following part number information for MPC860 processor.

CWH-UTP-PPCD-HE: CodeWarrior USB Tap for DPI Power Architecture


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply