CodeWarrior TAP tunnel across network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior TAP tunnel across network

2,556件の閲覧回数
smiller2
Contributor IV

Does CodeWarrior support tunneling across external networks to reach the TAP ?     What I want to do is setup my HW  with the CodeWarrior TAP connected to my local network and then have it tunnel to the Internet so it can be debugged remotely.    Segger and others provide this with a server application that runs on a local PC. 

Thanks.

0 件の賞賛
返信
3 返答(返信)

2,521件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior supports tunneling across external networks to reach the TAP.

0 件の賞賛
返信

2,553件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Smiller2,

Would you please let us know which NXP device you are using with Code Warrior?

Regards,
Gustavo

0 件の賞賛
返信

2,551件の閲覧回数
smiller2
Contributor IV

The part is the LS1046A.   The issue is DDR validation does not work correctly on this board.   However, the DIMM appears to work.    Given that I am not a CodeWarrior GURU,  my hope was to allow someone external, like an FAE, take control system and run DDR validation remotely to verify what I am seeing.

0 件の賞賛
返信