CodeWarrior TAP tunnel across network

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior TAP tunnel across network

2,618 Views
smiller2
Contributor IV

Does CodeWarrior support tunneling across external networks to reach the TAP ?     What I want to do is setup my HW  with the CodeWarrior TAP connected to my local network and then have it tunnel to the Internet so it can be debugged remotely.    Segger and others provide this with a server application that runs on a local PC. 

Thanks.

0 Kudos
Reply
3 Replies

2,583 Views
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior supports tunneling across external networks to reach the TAP.

0 Kudos
Reply

2,615 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Smiller2,

Would you please let us know which NXP device you are using with Code Warrior?

Regards,
Gustavo

0 Kudos
Reply

2,613 Views
smiller2
Contributor IV

The part is the LS1046A.   The issue is DDR validation does not work correctly on this board.   However, the DIMM appears to work.    Given that I am not a CodeWarrior GURU,  my hope was to allow someone external, like an FAE, take control system and run DDR validation remotely to verify what I am seeing.

0 Kudos
Reply