CodeWarrior IDE 5.9.0 exists?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior IDE 5.9.0 exists?

4,735 Views
sarangmujumdar
Contributor II

Hello,

I want to know about availability of CodeWarrior IDE ver. 5.9.0. for HC08 core microcontroller.

Also if it is available then where can I get its evaluation version to download?

can I install IDE 5.9.0 on Windows7 ?

 

Thanking you,

Labels (1)
7 Replies

4,383 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sarang,

It doesn't support the Win7,

CodeWarrior for Microcontrollers-Classic IDE|NXP  

pastedImage_2.png

There is a DOC about how to install it on Win7,you can have a try.

https://community.nxp.com/message/310577 

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,383 Views
sarangmujumdar
Contributor II

Hello Alice

Thank you for your support.

I am not yet sure whether IDE 6.3 supports HC08 processor like (MC68HC908AZ60) bcos it is not mentioned clearly in link you provided. Can you see it in Microcontroller list of IDE? please let me know....

pastedImage_1.png

0 Kudos
Reply

4,383 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sarang,

The CodeWarrior 6.3 is the CW IDE version 5.9 just like you said.

And yes, it support this chip : MC68HC908AZ60.

You can see this in the linker i mentioned :

pastedImage_1.png

Also i check the IDE :

pastedImage_2.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,383 Views
sarangmujumdar
Contributor II

Hello Alice

Thank you very much for your support. It is clear now on IDE version.

Only one query: I have Windows 7 on my computer so I have to refer following link you suggested

pastedImage_1.png

Have you tried to install IDE 6.3 on windows 7 by following procedure mentioned in above link?

Does IDE work faithfully if installed by this procedure ?

Best regards,

Sarang

0 Kudos
Reply

4,383 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Sarang,

Sorry , no, i haven't test it .

BR

Alice

0 Kudos
Reply

4,383 Views
sarangmujumdar
Contributor II

Hello Alice

Thank you very much for reply.

But I doubt that V10.7 Support HC08 Microcontroller. IDE 10.7 support S08, and HC(S)08 not HC08.

It seems it is only IDE 5.9.0. which has support for HC08 core .

But does IDE5.9.0. exist?  or is it discontinued?  please let me know.

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply

4,383 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sarang,

Sorry for the reply i have deleted,  i unexpected you received it so quickly , please ignore it .

Please refer to the response i just send to you .

BR

Alice

0 Kudos
Reply