CodeWarrior DEMOJM compatibility W7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior DEMOJM compatibility W7

1,350 次查看
chepoes
Contributor I

Hello, I have a problem, I own a DEMOJM board with the MCF51JM128 microcontroller. I used to work with Codewarrior 6.1 IDE version 5.0.9 because this was the softare included in a CD-ROM, running by Windows Vista 32-bit.

 

Now, I have to use the board now to develop an important project, but I have a new computer with Windows 7 64-bit. I tried to install the software included in my CD-ROM but a message appears telling Codewarrior is not compatible.

 

There is some way to work with DEMOJM board under windows 7? Please help.

标签 (1)
0 项奖励
回复
1 回复

1,266 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Antonio

Could you please refer to this thread?

CodWarrior unhandled exception

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复