CodeWarrior DEMOJM compatibility W7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior DEMOJM compatibility W7

1,348件の閲覧回数
chepoes
Contributor I

Hello, I have a problem, I own a DEMOJM board with the MCF51JM128 microcontroller. I used to work with Codewarrior 6.1 IDE version 5.0.9 because this was the softare included in a CD-ROM, running by Windows Vista 32-bit.

 

Now, I have to use the board now to develop an important project, but I have a new computer with Windows 7 64-bit. I tried to install the software included in my CD-ROM but a message appears telling Codewarrior is not compatible.

 

There is some way to work with DEMOJM board under windows 7? Please help.

ラベル(1)
0 件の賞賛
返信
1 返信

1,264件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Antonio

Could you please refer to this thread?

CodWarrior unhandled exception

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信