CodeWarrior 6.3 and Windows 7 64 bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 6.3 and Windows 7 64 bit

3,680件の閲覧回数
piergiovannigor
Contributor II

I wish to continue to use COdeWarrior 6.3, but it cannot be installed in a 64 bit machine.

Does exist a way to solve the problem ?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,639件の閲覧回数
RodneyMcGee
Contributor IV

I personally would not us XP mode. 

Here is how I use CW 6.3 natively on 7 and 10 64-bit. 

Install CodeWarrior Classic 6.3 Windows 10 & 7 64-bit HCS08 RS08 CFV1

Make sure to read the pinned comments and the video description. 

0 件の賞賛
返信

2,639件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Giovanni,

 

You could take a look to the following document that explains how to install and run Classic CodeWarrior products on 64-bit Windows 7 pc:

 

http://www.nxp.com/files/soft_dev_tools/doc/app_note/AN3936.pdf 

 

But please notice that we highly recommend you to use the eclipse based CodeWarrior version:

 

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 


Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信