CodeWarrior 6.3 and Windows 7 64 bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 6.3 and Windows 7 64 bit

3,760 Views
piergiovannigor
Contributor II

I wish to continue to use COdeWarrior 6.3, but it cannot be installed in a 64 bit machine.

Does exist a way to solve the problem ?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,719 Views
RodneyMcGee
Contributor IV

I personally would not us XP mode. 

Here is how I use CW 6.3 natively on 7 and 10 64-bit. 

Install CodeWarrior Classic 6.3 Windows 10 & 7 64-bit HCS08 RS08 CFV1

Make sure to read the pinned comments and the video description. 

0 Kudos
Reply

2,719 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Giovanni,

 

You could take a look to the following document that explains how to install and run Classic CodeWarrior products on 64-bit Windows 7 pc:

 

http://www.nxp.com/files/soft_dev_tools/doc/app_note/AN3936.pdf 

 

But please notice that we highly recommend you to use the eclipse based CodeWarrior version:

 

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 


Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply