CodeWarrior 11 compiler ISO26262 qualification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior 11 compiler ISO26262 qualification

2,071 次查看
phil74
NXP Employee
NXP Employee

Hello,

My customer is currently using CodeWarrior 11 for Qorivva/MPC56xx in a ISO26262 ASIL A project.

And they need to qualify the compiler.

 

Have you got some qualification data on this compiler, or proof of use (worldwide use in safety projects / number of customers)  that can help us on this topic ?

Or have you a contact person for this subject ?

 

Thank you in advance,
BR,

Philippe

 

标签 (1)
0 项奖励
回复
1 回复

1,923 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi phil74,

unfortunately, CodeWarrior 11 doesn't have any certifications.

We only have proven-in-use document which is signed by NXP CW product manager.

If you need it, please create a private case to CW team with the end customer information ( company, project,etc) to request it.

How to submit a new question for NXP Support 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复