CodeWarrior 10.6.4 for ColdFire linker errors after tool update

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior 10.6.4 for ColdFire linker errors after tool update

1,326 次查看
paul_carpenter
Contributor I

I previously compiled and linked a project with no errors (lots of warnings, yes, but no errors) with CodeWarrior v10.6.4 for ColdFire (5282).  I then had to reinstall CodeWarrior v10.6.4.  This time after the installation I decided to apply all of the suggested updates to the tool.  Now I cannot build the same project that used to build -- with absolutely no changes to source code, linked libraries, or project settings -- as I get linker errors about multiply-defined variables (see build output log below).  It seems these variables are rooted in the CodeWarrior tool chain, not in my source code, and appear to be related to math and/or floating point support...

Just to confirm nothing changed besides the tool I plan to uninstall CodeWarrior again and reinstall, but I will not apply the tool updates and see if the same project links again.

Does anyone have an idea of what's wrong and how to resolve this please?

Thanks.

Paul

'Building target: application_CW10.elf'
'Executing target #22 application_CW10.elf'
'Invoking: ColdFire Linker'
"C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf" @@"application_CW10.args" -o "application_CW10.elf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/RTOS/mcu/contrib/lib/C_4i_CF_StdABI_MSL.a" "-llibrt.a" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/RTOS/mcu/contrib/lib/fp_coldfire.o" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/RTOS/mcu/eos/CW10_6_out/eos.alf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/RTOS/mcu/libtimers/out/libtimers_CW10_6.alf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/RTOS/mcu/libdnp/out/libdnp_CW10_6.alf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/MCU/buildtemp/vm/vmmap_CW10.alf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/MCU/loglib/out/loglib_CW10.elf" -l"C:/SVNWork/PQ044_CCP9/013_SMS_Master_V3/branches/012_MCU_CW10_Upgrade/MCU/utllib/out/utllib_CW10.elf"
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\main.c|1577|0|0|0|0)
=
>Multiply-defined: "__double_huge" in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\MBSInterface.c|690|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DNPInterface.c|957|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SetpointScheduler.c|992|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SNTPClient.c|425|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\ScadaInterface.c|224|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DPRInterface.c|614|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DSPVMInterface.c|276|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\main.c|1577|0|0|0|0)
=
>Multiply-defined: "__extended_huge" in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\ScadaInterface.c|224|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DSPVMInterface.c|276|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SetpointScheduler.c|992|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SNTPClient.c|425|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DNPInterface.c|957|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DPRInterface.c|614|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\MBSInterface.c|690|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\main.c|1577|0|0|0|0)
=
>Multiply-defined: "__float_huge" in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\ScadaInterface.c|224|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DNPInterface.c|957|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DPRInterface.c|614|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\MBSInterface.c|690|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SNTPClient.c|425|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DSPVMInterface.c|276|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SetpointScheduler.c|992|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\main.c|1577|0|0|0|0)
=
>Multiply-defined: "__float_nan" in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DSPVMInterface.c|276|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SetpointScheduler.c|992|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\ScadaInterface.c|224|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\SNTPClient.c|425|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DNPInterface.c|957|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\DPRInterface.c|614|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
(C:\SVNWork\PQ044_CCP9\013_SMS_Master_V3\branches\012_MCU_CW10_Upgrade\MCU\src\MBSInterface.c|690|0|0|0|0)
=
>Previously defined in
C:/Freescale/CW MCU v10.6.4/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error
>Link failed.

Errors caused tool to abort.
mingw32-make: *** [application_CW10.elf] Error 1

0 项奖励
回复
1 回复

1,200 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

This issue was treated internally. It was a problem related with the migration of the project from Codewarrior classsic to Codewarrior eclipse based.

Regards

0 项奖励
回复