CodeWarrior 10.5.1 NOR-Flash task

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10.5.1 NOR-Flash task

2,047 Views
dmitrshard
Contributor II

Hello!

 

I work with custom board based on P3041 processor. Board have 512MB 32-bit NOR-Flash. I need to write u-boot to this flash. How i can do it?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,727 Views
lunminliang
NXP Employee
NXP Employee

Hello Dmitr Shard,

Also you could refer to AN4948 Flash Programmer for CodeWarrior Power Architecture.

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN4948.pdf?fsrch=1&sr=1&pageNum=1

Regards

Lunmin

0 Kudos
Reply

1,727 Views
addiyi
NXP Employee
NXP Employee

Please refer to Targeting_PA_Processors.pdf available in PA\Help\PDF\ or Flash Programmer for CodeWarrior Power Architecture .

Adrian

0 Kudos
Reply