CodeWarrior 10.5.1 NOR-Flash task

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 10.5.1 NOR-Flash task

2,000件の閲覧回数
dmitrshard
Contributor II

Hello!

 

I work with custom board based on P3041 processor. Board have 512MB 32-bit NOR-Flash. I need to write u-boot to this flash. How i can do it?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,680件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Dmitr Shard,

Also you could refer to AN4948 Flash Programmer for CodeWarrior Power Architecture.

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN4948.pdf?fsrch=1&sr=1&pageNum=1

Regards

Lunmin

0 件の賞賛
返信

1,680件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please refer to Targeting_PA_Processors.pdf available in PA\Help\PDF\ or Flash Programmer for CodeWarrior Power Architecture .

Adrian

0 件の賞賛
返信