CodeWarrior 10.5.1 NOR-Flash task

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior 10.5.1 NOR-Flash task

1,962 次查看
dmitrshard
Contributor II

Hello!

 

I work with custom board based on P3041 processor. Board have 512MB 32-bit NOR-Flash. I need to write u-boot to this flash. How i can do it?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,642 次查看
lunminliang
NXP Employee
NXP Employee

Hello Dmitr Shard,

Also you could refer to AN4948 Flash Programmer for CodeWarrior Power Architecture.

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN4948.pdf?fsrch=1&sr=1&pageNum=1

Regards

Lunmin

0 项奖励
回复

1,642 次查看
addiyi
NXP Employee
NXP Employee

Please refer to Targeting_PA_Processors.pdf available in PA\Help\PDF\ or Flash Programmer for CodeWarrior Power Architecture .

Adrian

0 项奖励
回复