Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board

1,700 Views
weikun
Contributor I

Hi,

I have installed code warrior v10.6.4 in my laptop with windows 10 system, using USB TAP, when debug, it can not connect to 56F8013 based board. my ccs version is 4.13. it occurs the following: 

ccsfigure.png

how can I fix it?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,521 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

USB tap 4.13 can work with CW10.6.4  on 64bit win10 without problem.

Can you please test your usb tap on another computer with other board,if the usb tap is in good condition and not be damaged?

Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply