code warrior DSC V8.3 special edition in windows 8 64 bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code warrior DSC V8.3 special edition in windows 8 64 bit

1,582 Views
arunrajk
Contributor I

I installed code warrior DSC V8.3 special edition in windows 8 64 bit  i can't open the processor expert component wizard. any one suggest me the solution.

0 Kudos
Reply
1 Reply

1,442 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

according to CodeWarrior Factsheet, http://www.nxp.com/docs/en/fact-sheet/950-00437.pdf 

processor expert component wizard is not available in CodeWarrior for DSC.

Besides, CodeWarrior for DSC v8.3 doesn't support  64bit win8, it supports "Windows® XP/Vista 32-bit (Home Premium Edition & Business Edition)", if you want to wort with DSC, please use CW v10.7 instead.

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply