Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code warrior + USB TAP in Window 10 system can not connect to 56F8013 based board

1,681件の閲覧回数
weikun
Contributor I

Hi,

I have installed code warrior v10.6.4 in my laptop with windows 10 system, using USB TAP, when debug, it can not connect to 56F8013 based board. my ccs version is 4.13. it occurs the following: 

ccsfigure.png

how can I fix it?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

USB tap 4.13 can work with CW10.6.4  on 64bit win10 without problem.

Can you please test your usb tap on another computer with other board,if the usb tap is in good condition and not be damaged?

Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信