Code warrior 5.9.0 in CodeWarrior Development Tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code warrior 5.9.0 in CodeWarrior Development Tools

3,214 Views
ravadasrikanth3
Fresh Out Contributor

Hi sir,

We are using the code warrior 5.9.0 version for the tower kit (TWR MPC5125 ). we didn't find the device MCP5125. Would you please help us to in which version the device is available then explain steps to how we will proceed further.

thank you sir

Best regards

Srikanth 

Labels (1)
0 Kudos
Reply
3 Replies

2,968 Views
Pavel
NXP Employee
NXP Employee

Install SP1 patch for the MPC5125. Load this patch using the following link to Google drive:

https://drive.google.com/open?id=1vQAgW6Dj7aNxCVYszgi2hObyClR67yzS


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,968 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

To work with MPC5125, we use CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2. Here is the download page

CodeWarrior® Development Tools for mobileGT®|NXP 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,968 Views
ravadasrikanth3
Fresh Out Contributor

hi sir,

we already used codeWarrior for mobileGT Linux Application Edition (Windows Hosed) v9.2 only. In that help section we didn't find the MPC5125 device .What can we do ? 

0 Kudos
Reply