Code warrior 5.9.0 in CodeWarrior Development Tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code warrior 5.9.0 in CodeWarrior Development Tools

3,150件の閲覧回数
ravadasrikanth3
Fresh Out Contributor

Hi sir,

We are using the code warrior 5.9.0 version for the tower kit (TWR MPC5125 ). we didn't find the device MCP5125. Would you please help us to in which version the device is available then explain steps to how we will proceed further.

thank you sir

Best regards

Srikanth 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,904件の閲覧回数
Pavel
NXP Employee
NXP Employee

Install SP1 patch for the MPC5125. Load this patch using the following link to Google drive:

https://drive.google.com/open?id=1vQAgW6Dj7aNxCVYszgi2hObyClR67yzS


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,904件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

To work with MPC5125, we use CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2. Here is the download page

CodeWarrior® Development Tools for mobileGT®|NXP 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,904件の閲覧回数
ravadasrikanth3
Fresh Out Contributor

hi sir,

we already used codeWarrior for mobileGT Linux Application Edition (Windows Hosed) v9.2 only. In that help section we didn't find the MPC5125 device .What can we do ? 

0 件の賞賛
返信