Code Warrior for MPC8640 single core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior for MPC8640 single core

1,349 Views
richleone
Contributor I

Does anybody know if code warrior will work with a single core MPC8640?

0 Kudos
Reply
1 Reply

1,188 Views
alexander_yakov
NXP Employee
NXP Employee

As far as I can see, MPC8640 is not listed in CodeWarrior interface, but you can use "MPC8641D" as this device is very close (based on the same silicon and covered by the same silicon errata document).

MPC8641D is supported by CodeWarrior for Power Architecture v8.8 (Classic IDE)

 

CodeWarrior Dev Tools for Networked Apps|NXP 

At this page please find "CodeWarrior Power Architecture for MPC8xx, MPC7xxx, and most MPC8xxx PowerQUICC processors"


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply