Code Warrior for MPC8640 single core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior for MPC8640 single core

1,293件の閲覧回数
richleone
Contributor I

Does anybody know if code warrior will work with a single core MPC8640?

0 件の賞賛
返信
1 返信

1,132件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

As far as I can see, MPC8640 is not listed in CodeWarrior interface, but you can use "MPC8641D" as this device is very close (based on the same silicon and covered by the same silicon errata document).

MPC8641D is supported by CodeWarrior for Power Architecture v8.8 (Classic IDE)

 

CodeWarrior Dev Tools for Networked Apps|NXP 

At this page please find "CodeWarrior Power Architecture for MPC8xx, MPC7xxx, and most MPC8xxx PowerQUICC processors"


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信