Code Warrior 10.6 Licensing Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior 10.6 Licensing Issue

2,291件の閲覧回数
kiranbhat
Contributor III

Hi

I am using code warrior development suite professional with perpetual floating license. The license status is active but while compiling gives the error on code limit. Screen shot of the license status and the error is attached.

 

Thanks
Regards

 

 

Kiran bhat

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,124件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Kiran

There is some problem in your license installation.  Please follow the instructions in the attached document to install floating license.

If this does not help, would you please try to ping the IP address of the server? Whether the host can connect server? And also check whether the license server for CodeWarrior is started in FlexIM? Please also exit firewall on host.

I would suggest submitting a case. It's better under case process for private license details. For how to do it, please refer to:

https://community.freescale.com/docs/DOC-330215

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,124件の閲覧回数
kiranbhat
Contributor III

Hi Fiona

Thanks for the support. I just changed the project workspace and it worked fine dont know the exact issue. This issue occurred 2 times in different PC's.

Regards

Kiran Bhat

0 件の賞賛
返信