Code Warrior 10.6 Licensing Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code Warrior 10.6 Licensing Issue

2,365 次查看
kiranbhat
Contributor III

Hi

I am using code warrior development suite professional with perpetual floating license. The license status is active but while compiling gives the error on code limit. Screen shot of the license status and the error is attached.

 

Thanks
Regards

 

 

Kiran bhat

标签 (1)
0 项奖励
回复
2 回复数

2,198 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Kiran

There is some problem in your license installation.  Please follow the instructions in the attached document to install floating license.

If this does not help, would you please try to ping the IP address of the server? Whether the host can connect server? And also check whether the license server for CodeWarrior is started in FlexIM? Please also exit firewall on host.

I would suggest submitting a case. It's better under case process for private license details. For how to do it, please refer to:

https://community.freescale.com/docs/DOC-330215

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,198 次查看
kiranbhat
Contributor III

Hi Fiona

Thanks for the support. I just changed the project workspace and it worked fine dont know the exact issue. This issue occurred 2 times in different PC's.

Regards

Kiran Bhat

0 项奖励
回复