Code Warrior 10.6 Licensing Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior 10.6 Licensing Issue

2,364 Views
kiranbhat
Contributor III

Hi

I am using code warrior development suite professional with perpetual floating license. The license status is active but while compiling gives the error on code limit. Screen shot of the license status and the error is attached.

 

Thanks
Regards

 

 

Kiran bhat

Labels (1)
0 Kudos
Reply
2 Replies

2,197 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Kiran

There is some problem in your license installation.  Please follow the instructions in the attached document to install floating license.

If this does not help, would you please try to ping the IP address of the server? Whether the host can connect server? And also check whether the license server for CodeWarrior is started in FlexIM? Please also exit firewall on host.

I would suggest submitting a case. It's better under case process for private license details. For how to do it, please refer to:

https://community.freescale.com/docs/DOC-330215

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,197 Views
kiranbhat
Contributor III

Hi Fiona

Thanks for the support. I just changed the project workspace and it worked fine dont know the exact issue. This issue occurred 2 times in different PC's.

Regards

Kiran Bhat

0 Kudos
Reply