Cannot complete the install Service Pack for Wireless Charging MWCT101x 1.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot complete the install Service Pack for Wireless Charging MWCT101x 1.0.1

Jump to solution
4,147 Views
rla00220
Contributor III

I encountered an error while installing Code Warrior to build wct1013a.

I get an error when I download the service pack and install the zip file.

  Missing requirement: MCU v10.7 DSC Service Pack for Wireless Charging MWCT101x 1.0.1 (com.freescale.mcu10_7.Wireless_Charging_MWCT101x.win.sp.feature.group 1.0.1) requires 'com.freescale.mcu10_7.product [1.0.0,20.0.0.RT5]' but it could not be found.

what should i do?

0 Kudos
Reply
1 Solution
3,993 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Semi,

Here is the point you need pay attention:

- during install CW10.7, please sure DSC component is selected

pastedImage_2.png

- open on line update page, make sure DSP support and MCU v10.7 DSC Service Packs are updated, if not, please update them.

pastedImage_3.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,994 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Semi,

Here is the point you need pay attention:

- during install CW10.7, please sure DSC component is selected

pastedImage_2.png

- open on line update page, make sure DSP support and MCU v10.7 DSC Service Packs are updated, if not, please update them.

pastedImage_3.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,672 Views
joshivaldi
Contributor II

Hello,

 

I followed your instructions and got this message when installing MCU v10.7 DSC Service Pack

 

"Cannot complete the install because one or more required items could not be found.
Software being installed: MCU v10.7 DSC Service Pack for DSC MC56F82xx6 1.0.1 (com.freescale.mcu10_7.DSC_MC56F82xx6.win.sp.feature.group 1.0.1)
Missing requirement: MCU v10.7 DSC Service Pack for DSC MC56F82xx6 1.0.1 (com.freescale.mcu10_7.DSC_MC56F82xx6.win.sp.feature.group 1.0.1) requires 'com.freescale.mcu10_7.product [1.0.0,20.0.0.RT5]' but it could not be found"

joshivaldi_0-1713316375956.png

 

Is CW v10.5 Still available? I am looking to use the MWCT1000CFM library.

CW MCU v10.5 Wireless Charging MWCT1xxx Service Pack (nxp.com)

 

 

0 Kudos
Reply