Can't open my project anymore

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't open my project anymore

Jump to solution
3,576 Views
MAPC
Senior Contributor I

Hello, dears

 

My project was running ok. Suddenly, when I open Code Warrior 10.5, it pops us the following message:

 

11914_11914.jpgproj_open_error.jpg

 

And since then, I just can't open the project anymore. When I close a message, another one comes up, and this never ends. It is curious that this happens with only one project in my workspace. The other project can be opened without problems. I couldn't identify the reason for that. Probably, one or more files might be corrupted, I don't know.

 

Did anybody face such a problem?

 

 

Regards,

 

Marco Coelho

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
3,261 Views
BlackNight
NXP Employee
NXP Employee

It might be something with the parallel build settings?

Can you try the fix mentioned in CW ProjectsView Project Loading Verification Internal Error

?

View solution in original post

0 Kudos
Reply
3 Replies
3,261 Views
MAPC
Senior Contributor I

Hi, Erich

I just tried it and worked perfectly.

The doesn't ocurr only with QG8. In my project, I used MC9S08PA8. It seems like a kind of bug in Code Warrior v. 10.5?

I hope that was solved in Code Warrior v. 10.6.

Thank you very much!

Marco Coelho

0 Kudos
Reply
3,262 Views
BlackNight
NXP Employee
NXP Employee

It might be something with the parallel build settings?

Can you try the fix mentioned in CW ProjectsView Project Loading Verification Internal Error

?

0 Kudos
Reply
3,261 Views
MAPC
Senior Contributor I

Hi, Erich

I just tried it and worked perfectly.

The doesn't ocurr only with QG8. In my project, I used MC9S08PA8. It seems like a kind of bug in Code Warrior v. 10.5?

I hope that was solved in Code Warrior v. 10.6.

Thank you very much and congratulations for your valuable job on mcuoneclipse.com!

Marco Coelho

0 Kudos
Reply