Can't connect to GDB proxy on CodeWarrior TAP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't connect to GDB proxy on CodeWarrior TAP?

3,186 次查看
mdavis331
Contributor I

Experiencing the same problems as this post (https://community.nxp.com/thread/315425#362363)

Suggested resolution: "As it turned out, for some reason, gdbproxy did not start in the TAP. A delete followed by config cc cwtap via CCS, re-spawn  the gdbproxy and now it works fine."

Where can I find the tools to execute the following instructions? I do not possess CodeWarrior and attempted to download the evaluation versions:

1) CodeWarrior® Development Studio for mobileGT® - could not successfully install

2) CodeWarrior® Development Studio for MPC5xx - did not find the CCS utilities

I can successfully connect and communicate to the CodeWarrior TAP via Telnet. Verified per this post (https://community.nxp.com/message/977831) that I possess all necessary documentation and I am configuring GDB properly when attempting to connect. Exact commands on host PC running GDB (from processorID_init.gdb):

  • set logging off
  • set debug frame 0
  • set debug remote 0
  • set remotetimeout 100
  • target remote myTargetIPAddress:2345

Result: same as post referenced above (https://community.nxp.com/thread/315425#362363)

0 项奖励
回复
2 回复数

2,650 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthew Davis,

If you are using QorIQ PowerPC processors, please download and install CodeWarrior for PowerPC 10.5.1 from CodeWarrior Dev Tools for Networked Apps|NXP, CCS is in C:\Freescale\CW_PA_v10.5.1\PA\ccs\bin.

If you are using QorIQ Layerscape ARMv8 processors, please download and install CodeWarrior for ARMv8 from CodeWarrior Dev Tools for Networked Apps|NXP, CCS is in C:\Freescale\CW4NET_v2017.03\Common\CCS\bin.

If you are using LS102x processor, please download and install CodeWarrior for ARMv7 from CodeWarrior Dev Tools for Networked Apps|NXP, CCS is located in C:\Freescale\CW4NET_v2017.03\Common\CCS\bin.

We provided boards bringing up support with GDB and CodeWarrior TAP several days ago when we just started to use
CodeWarrior TAP to replace USB TAP. The document and gdb test tar ball containing boards initialization and configuration files released at that time are old, only can be used on PowerPC platforms. Then we didn't provide any
update release to customers, so we don't have gdb configuration demos for Layerscape(ARM core) processors, because we recommend customers to purchase CodeWarrior license.

For documents, you could refer to
CWTAP_GDB_GSG.pdf provided by Pavel Chubakov in https://community.nxp.com/thread/468025,

We have GDB configuration demos tar ball working with CodeWarrior TAP for PowerPC platforms, please refer to gdb_test_ccs_365 provided in the above link. If users still want to use GDB and CodeWarrior TAP to do QorIQ Layerscape brining up, they could create their own initialization and configuration files based on the existing demos for PowerPC referring to CodeWarrior initialization file.
Please refer to the video provided in http://www.nxp.com/video/board-level-bringup-using-codewarrior-tap-and-gdb:BOARDLVL_CWTAPGDB_VID.


GDB proxy setting up section is provided in the script bin/<platform>_init.gdb, after setting up gdb console, you could run the following command to connect to the target board.(gdb) source p4080_init.gdb
Please refer to the following commands to connect to gdb proxy.
(gdb) set logging off
(gdb) set debug frame 0
(gdb) set debug remote 0
(gdb) set remotetimeout 100
(gdb) set tdesc filename ../xml/power-core.xml
(gdb) target remote 10.193.20.72:2345
Remote debugging using 10.193.20.72:2345
0x00000000 in ?? ()
(gdb) mon get_probe_status
Connected to gdbserver FSL039B85:2345


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,650 次查看
mdavis331
Contributor I

Hello Yinping!

Thank you for the response. My team and I were able to correctly initialize and communicate the GDB proxy given the information above. We still need some assistance with a particular instruction. Specifically:

mon jtag_chain <myTarget_ID>

Where can I locate the correct myTarget_ID for MPC 8240 and MPC 8245?

0 项奖励
回复