Can I use my usb dongle on a 64-bit Windows 7 machine?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use my usb dongle on a 64-bit Windows 7 machine?

1,526 次查看
eesso
Contributor I

I recently bought a usb dongle and need a license for it. My company has already purchased 2x floating licence. 

1. Can I convert one of the floating licences to a usb dongle licence?

2. Can I use my usb dongle on a 64-bit Windows 7 machine? I see this note USB Dongle | NXP 

Note: With our classic CodeWarrior IDE products, we do not support USB dongle license configurations for 64-bit Windows 7 and Linux host OS

3. What is the classic Code Warrior IDE products? Does this include Code Warrior Development Suite for Networked Applications? What are my options if I need to use Code Warrior application without access to the license server on a 64-bit Windows 7 machine?

 

标记 (1)
0 项奖励
回复
1 回复

1,464 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Classic CW doesn't support dongle license on 64bit win7.

For CW4NET product, our recommendation is to use node lock license or floating license.

It seems CW4NET product doesn't have option of bounding with dongle on license management web page.

If you have this requirement, please create a ticket to license support team.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复