CW10 & P&E Cyclone FX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10 & P&E Cyclone FX

1,649 Views
silentsam
Contributor II
Operating System: Windows 10 64-bit
- Using CW10 to debug NXP TMPS hardware; specifically the 
FXTH87 TPMS microchip.
- Target is powered via seperate DC power supply; 2.5V, 25mA.
- All latest P&E driver updates are installed. 
- Debugger is visible and is automatically selected in CW10.
- Tried playing with debug configurations, each time recieve the same dialog box with error
stating the target has not been detected.

Has anyone else had a similar issue when using this debugger with CW10?

thanks in advance,

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,542 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Please check community content in the following link: https://community.nxp.com/message/600009

 

Seems like there was a similar problem in this community thread and it was solved by choosing the following configuration when creating the project for the FXTH87: select S08->FXTH8700 Family> FXTH870000.

 

If this does not solve your case, I would recommend you to add the detailed issue you are facing (including screenshots of the error message) in that same community thread.

0 Kudos
Reply