CW: workspace binding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW: workspace binding

ソリューションへジャンプ
2,380件の閲覧回数
svenmoeller
Contributor II

Hello,

 

do i always have to set up a new workspace to edit a new project?

 

I just wonder if it is possible to create a kind of project file like those:

  • .eww in IAR Embedded Workbench
  • .sln in MS Visual Studio

 

Are there any possibilities to be not bound to workspaces in CW?

 

Thank you

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,265件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,265件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

0 件の賞賛
返信