CW: workspace binding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW: workspace binding

Jump to solution
2,349 Views
svenmoeller
Contributor II

Hello,

 

do i always have to set up a new workspace to edit a new project?

 

I just wonder if it is possible to create a kind of project file like those:

  • .eww in IAR Embedded Workbench
  • .sln in MS Visual Studio

 

Are there any possibilities to be not bound to workspaces in CW?

 

Thank you

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,234 Views
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

View solution in original post

0 Kudos
Reply
1 Reply
2,235 Views
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

0 Kudos
Reply