CW: workspace binding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW: workspace binding

跳至解决方案
2,278 次查看
svenmoeller
Contributor II

Hello,

 

do i always have to set up a new workspace to edit a new project?

 

I just wonder if it is possible to create a kind of project file like those:

  • .eww in IAR Embedded Workbench
  • .sln in MS Visual Studio

 

Are there any possibilities to be not bound to workspaces in CW?

 

Thank you

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,163 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,164 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

you do not need a new workspace for a new project. A workspace is simply a container for projects and settings.

You do not need to have the project in the workspace (folder) itself, they can be anywhere.

Erich

0 项奖励
回复