CW license with unknow error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW license with unknow error

3,986 Views
paul_han
Contributor I

A basic version of CW:

Part Description: CodeWarrior Development Suite - Basic Edition, Annual Subscription, Floating License

is purchased and registered. A license.dat is generated and placed in the MCU directory. CW 10.7 has proceduced a unknown error,

Here is the detail:

Detail information for product "CodeWarrior for MCU" version "10.7.0.FSL_b06017"
status: "Unknown error with key BasicEditionMCU 10.5, LM_NOT_THIS_HOST.  "
License model: "class com.freescale.core.ide.license.flexlm.FlexlmActivate11"
Contact Email: [email protected]
Register URL: http://www.freescale.com/cwregister
Purchase URL: http://www.freescale.com/cwmcu10
FlexLM Eval Period: 15 day(s)
GTL Server: gtlsrvr.metrowerks.com
GTL Port: 80 (8,080)
Wants Host ID: true
License file path: C:\Freescale\CW MCU v10.7\MCU\license.dat
flexlmFileLocator: null
flexlmFile: ${MCU_TOOLS_HOME}/license.dat
License file URL: file:/C:/Freescale/CW MCU v10.7/eclipse/../MCU/license.dat
Error String: Unknown error with key BasicEditionMCU 10.5, LM_NOT_THIS_HOST.  
Mandatory feature keys:
    BasicEditionMCU 10.5, status : Unknown error with key BasicEditionMCU, LM_NOT_THIS_HOST.
Alternate Keys:
(no keys)
LM_PATH=null
License file Content (C:\Freescale\CW MCU v10.7\MCU\license.dat):
 #CodeWarrior Development Suite - Basic Edition, Annual Subscription, Floating
#License - CodeWarrior for MCU Basic Edition (Windows - Eclipse) for Paul Han
#Software Account
SERVER this_host DISK_SERIAL_NUM=xxxxxxxx
VENDOR metrowks
USE_SERVER
INCREMENT BasicEditionMCU metrowks 10.5 04-jan-2018 1 xxxxxxxxxxxxx \
    VENDOR_STRING="CodeWarrior for MCU Basic Edition (Windows - \
    Eclipse)" DUP_GROUP=UH ISSUER="Freescale Semiconductor" \
    ISSUED=04-jan-2017 ck=116 SN="FSL - xxxxxxxx" TS_OK

 

Can someone help ASAP please.

 

Thanks.

 

 

Paul

Labels (1)
0 Kudos
Reply
5 Replies

3,451 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,451 Views
paul_han
Contributor I

Great, It worked.

Thanks for your help,

Have a good weekend,

Paul Han

0 Kudos
Reply

3,451 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Paul,

You use floating license. Please follow this doc to install floating license step by step

Step Byt Step Screenshot Guide Floating license FlexLM for CodeWarrior.pdf 

Regarding the original download license file, you need Make the following changes to your license file.

 

FROM: this_host

TO: Your license server's host IP address, or your license server's host name

 

If this can not solve your problem, because this involved your private asset, please create a private ticket with your license.dat. the engineer for license will check it.

https://community.nxp.com/docs/DOC-329745 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,451 Views
paul_han
Contributor I

Hi Jennie,

Thanks for your reply.

We followed with the instruction and got most of license installed. There is a problem we have on the port used for the license. port 27000 (in the Server status tab the perform Status Enquiry returns the license info for NI Labview) is used. Can we use any port or has to be 27000? Is it possible to use a different port for the NCP licenses?

Thanks,

Paul

0 Kudos
Reply

3,451 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Yes, I ever used port 1700. It works fine on my side.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply